Define the Pipe Fill Settings for a Mimic

You can use the Pipe Fill tab of the Mimic Properties window to define the default settings for the background of pipes that you add to Mimics. This is useful when you know that you need to add multiple pipes to a Mimic, each with the same color or style of background. Rather than configure the fill settings for each pipe separately, you can define the default fill settings for pipes. After doing this, each pipe that you add will already have the default fill settings in place. You can make further adjustments to each pipe by configuring its own settings separately if required.

Depending on the method that you use to display the Mimic Properties window, the settings you define will be applied to:

When you have displayed the Mimic Properties window using the appropriate method for your needs, define the Pipe Fill settings as required. The various Pipe Fill settings work in the same way as the similarly named settings on the Fill tab of the Pipe Properties window (see Editing a Pipe).


Disclaimer

Geo SCADA Expert 2022