Embed an X-Y-Z Plot on a Mimic

You can embed X-Y-Z Plots on your Mimics. Embedded X-Y-Z Plots update in the same way as X-Y-Z Plots that are stored as database items and provide similar advantages to embedded Mimics:

To embed an X-Y-Z Plot on a Mimic:

  1. Display the Mimic that is to contain the embedded X-Y-Z Plot. You need to display the Mimic in Design mode (see Displaying a Mimic).
  2. Select X-Y-Z Plot in the Drawing command group on the Graphics Tab.

    The Select X-Y-Z Plot window is displayed.

  3. Navigate to the required X-Y-Z Plot in the window, and then press the OK button.
  4. Draw the outline of the embedded X-Y-Z Plot by pressing the left-hand mouse button, and moving the cursor while keeping the left-hand mouse button pressed. The rectangle that is drawn is the space that will be occupied by the embedded X-Y-Z Plot.

Alternatively:

  1. Display a Mimic in Design mode (see Displaying a Mimic).
  2. Display the Database Bar (see Display an Explorer Bar).
  3. In the Database Bar, select the X-Y-Z Plot that you want to embed and drag it onto the Mimic.
    A context-sensitive menu is displayed.
  4. Select the Embedded X-Y-Z Plot option to embed the X-Y-Z Plot on the Mimic.

You can resize the embedded X-Y-Z Plot by selecting it and dragging its sides. Similarly, you can reposition it by selecting it and dragging it to a new position.

You can edit the embedded X-Y-Z Plot by double-clicking on it (see Editing an Embedded X-Y-Z Plot). You can also access editing features by right-clicking on the embedded X-Y-Z Plot to display a context sensitive menu (see Mimic Editing Features).


Disclaimer

Geo SCADA Expert 2022