Pie Chart Animations
You can animate the following properties for pie charts:
- Font—Represents the text properties of the labels, values, and percentages shown in the key for the pie chart. These properties work in the same way as Font Animations.
- Key Pos—Use to animate the position of the pie chart's key (see Key Pos).
- Key Style—Use to animate the type of key that is shown for the pie chart (see Key Style)
- PickComment—see PickComment Animations.
- PickDisabled—see PickDisabled Animations.
- PickParam—see Pick Action Animations for Mimic Objects if you are configuring a pie chart on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring a pie chart on a Symbol Mimic.
- PickType—see Pick Action Animations for Mimic Objects if you are configuring a pie chart on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring a pie chart on a Symbol Mimic.
- PosAnchor—see Rotation Animations.
- PosMax—see Rotation Animations.
- PosMin—see Rotation Animations.
- PosVal—see Rotation Animations.
- Slice01 - Slice10—Use to associate each slice of the pie chart with a value (see Slice Animations).
- ToolTipText—see ToolTipText Animations.
- Visible—see Visibility Animations.