In ViewX, you can display Mimics in two modes:
Run Mode
When a Mimic is displayed in Run Mode, its operational features are active. For example, hyperlinks can be selected and will cause other displays to be shown, and animated values will update in real-time. Run Mode is usually the active mode for Mimics in control rooms and so on, where they are used by operator level users to interact with the system.
The Mimic configuration-related features are unavailable when a Mimic is displayed in Run Mode. You cannot configure any Mimic objects when a Mimic is in Run mode, even if your User account has the Configure permission.
Design Mode
When a Mimic is displayed in Design Mode, its configuration features are active. For example, if you select a hyperlink, you access the configuration settings for the hyperlink rather than trigger the hyperlink to show the target display.
                    
Typically, operator level users have accounts that restrict their access to configuration features, so they will only use Mimics in Run Mode. Engineers often have the Configure permission and so can access both Run Mode and Design Mode.
If you are configuring a Mimic and need to test whether pick actions, animations and so on work, you will need to switch the Mimic from Design Mode into Run Mode. This is because pick action menus and animations are only active in Run Mode.
To switch between the two modes, either:
- Select the Design Mode button 
     on the Quick Access Toolbar. on the Quick Access Toolbar.The Design button switches between Run Mode and Design Mode (when it appears with a green background, the Mimic is in Design Mode). 
Or:
- Select the Design Mode command  on the ViewX ribbon's Edit tab. on the ViewX ribbon's Edit tab.
In Virtual ViewX, you can only display Mimics in Run Mode. To configure a Mimic, you have to use a ViewX client.