Edit Tab

The Edit tab contains the following command groups:

The Save, Clipboard and Undo /Redo groups include commands that mainly apply to users with higher security permissions. The exception to this is the Save in Document Store command, which you can use to Add a Copy of a Document to your Operator Document Store.

Copy and Paste limitations apply when you are using a Virtual ViewX client (see Use Copy and Paste in Virtual ViewX).

The Export group includes the Export command. You use this command to export data from Queries and Trends. This option is useful to export high volume of data from ViewX and Virtual ViewX where you do not have an option to copy the data to clipboard. You can only use the Export command when you run Virtual ViewX in Full Virtual ViewX mode. By default, the data is exported in 'Text (Tab delimited)' format. For more information, see Queries Lists and see Copy Trend Data to the Clipboard.

 

The Design group includes the Design Mode command, used by high-level users to switch between Run Mode and Design Mode while configuring database items.


Disclaimer

Geo SCADA Expert 2022