Use Copy and Paste in Virtual ViewX
When using Virtual ViewX, be aware that you cannot use Copy and Paste buttons or menu options in Geo SCADA Expert to copy content from Virtual ViewX into another application. This is a browser security feature. To copy content from Virtual ViewX into another application, such as Notepad, you have to use the keyboard shortcuts or the menu options provided by the web browser. The keyboard shortcuts that you can use include:
| Keys | Action |
|---|---|
| CTRL + A | Selects all of the content in the active field |
| CTRL + C | Copies the selected content to the local machine's clipboard |
| CTRL + V | Pastes the copied content from the clipboard |
When running Virtual ViewX in Full Virtual ViewX mode, an Export command is available on the Edit tab of the ViewX ribbon. You can use the Export command to export the data for all of the traces. By default, the data is exported in 'Text (Tab delimited)' format.
Further Information
Copy and paste status attribute content: see Use the Status Display Buttons.