Configuring Analog Points

The Mitsubishi driver supports Analog Input and Analog Output points.

Configure the properties for each analog point using the fields on the Mitsubishi Analog Point Form.

This section covers configuration of Mitsubishi-specific properties on the Mitsubishi tab of the Form.

Use the Mitsubishi tab to:

For information on the fields on the Analog tab, see Defining Analog Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2022