Geo SCADA Expert Advanced Modbus Driver

The Advanced Modbus driver supports additional functionality to the Simple Modbus driver, including:

If both drivers provide the required functionality, consider using the Advanced Modbus driver rather than the Simple Modbus driver. Using the Advanced Modbus driver will give you more flexibility should your system requirements change in the future.

For more information about the Advanced Modbus driver, see the Geo SCADA Expert Guide to the Advanced Modbus Driver.


Disclaimer

Geo SCADA Expert 2022