Configuring Analog Points

The Simple Modbus driver supports Analog Input and Analog Output points.

Analog points can be physical points that exist on Modbus PLCs, or calculated values that reside within Modbus registers.

Configure the properties for each analog point using the fields on the Simple Modbus Analog Point Form.

This section covers configuration of properties on the Modbus tab of the Form.

Use the Modbus tab to:

For information on the fields on the Analog Point tab, see Defining Analog Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.

For examples showing how to configure analog points to fulfill Modbus scanning requirements, see Configuration Examples.


Disclaimer

Geo SCADA Expert 2022