Configuring Analog Points

The Simple OPC driver supports Analog Input and Analog Output points.

The points are used to map ‘point’ data on OPA servers into Geo SCADA Expert in a format that it can understand, and vice versa.

Configure the properties of each analog point using the fields on the Simple OPC Analog Point Form.

This section covers configuration of analog-specific properties on the OPC tab of the Form.

Use the fields on the OPC tab to:

For information on the fields on the Analog Point tab, see Defining Analog Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2022