OPC UA Servers List

The OPC UA Servers List is specific to the OPC UA driver - it is only available on systems on which that driver is installed. Like other Queries Lists, you can display the List from the Queries Bar.

The OPC UA Servers List provides a summary of the status of the OPC UA Server database items to which your User Account and the client provide access.

As with other Lists, the OPC UA Servers List consists of rows and columns. Each row represents an individual OPC UA Server and each column contains status information about that particular OPC UA Server item.

The OPC UA Servers List contains these columns:

As with other Lists, you can right-click on an entry in the List to display a context-sensitive menu. From this menu, you can select options to display further information about an OPC UA Server, or perform various actions. For information about the actions that are specific to this type of database item, see Actions Associated with OPC UA Servers.


Disclaimer

Geo SCADA Expert 2022