Display the Pager Channel Form

Each Pager Channel database item has a configuration Form that you can use to define the various properties for the channel.

To display the Pager Channel Form, right-click on the Pager Channel database item in the Database Bar, then select the Edit Properties option. You need to be logged on via a User account that has the Configure Database permission. (If the Pager Channel item does not already exist in the database, you will need to Create a Pager Channel Database Item.)

There are several other ways of displaying a Form for a database item (see Display a Form in the Geo SCADA Expert Guide to Core Configuration).

When you have displayed the Form for your Pager Channel database item, you can use it to define the properties for the channel. For more information, see:


Disclaimer

Geo SCADA Expert 2022