Introduction to the SCADAPack Modbus Driver

This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring SCADAPack Modbus items and features in the Geo SCADA Expert database.

The guide also contains information for:

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s SCADAPack Modbus driver. The SCADAPack Modbus driver is an Advanced ModbusExtension Driver. It provides additional functionality to enable Geo SCADA Expert to communicate with SCADAPack® controllers, using the Modbus® protocol suite (see Which Driver?). In order to communicate with SCADAPack controllers, Geo SCADA Expert needs to run both the Advanced Modbus driver and the SCADAPack Modbus extension driver (see Confirm that the SCADAPack Modbus Server Component is Installed).

The Modbus communication types that the driver supports include:

Geo SCADA Expert can communicate with SCADAPack controllers directly, using direct or PSTN communications. Function codes supported by the SCADAPack Modbus driver determine how it reads or writes to data on the controllers (see Modbus Function Codes Supported by the Geo SCADA Expert SCADAPack Modbus Driver).

Geo SCADA Expert can also provide a communications ‘gateway’ to allow applications such as Telepace®, and ISaGRAF®, to communicate with SCADAPack controllers remotely, via the same communications link (for example, in situations where a SCADAPack controller has only one radio link). With the latter set-up, a Remote Connection database item provides a TCP/IP socket connection between Geo SCADA Expert and the remote application.

The SCADAPack Modbus driver also enables Geo SCADA Expert to retrieve DLOG (stored SCADAPack) data records from SCADAPack controllers and, if required, store those records historically in the Geo SCADA Expert database.

The SCADAPack Modbus driver documentation:

The documentation also explains:

If your Geo SCADA Expert system is running the SCADAPack Modbus Realflo Extension Driver to communicate with SCADAPack controllers that have Realflo enabled, it will support additional features that only apply to the Realflo-enabled devices. Use the Geo SCADA Expert Guide to the SCADAPack Modbus Realflo Driver in conjunction with this guide for information on these additional features.


Disclaimer

Geo SCADA Expert 2022