Pulse Meter Input Type

The Meter Input tab fields vary depending on the Meter Input Type that you select. This sections describes the fields related to either the Mass (Pulse) or Volume (Pulse) Meter Input Type. (The latter type of meter input only applies to Liquid and Water Flow Runs.)

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

The input alarms fields allow you to set the alarm thresholds for alarm types that have been enabled in the Inputs section on the Flow Run tab.

Use the following to configure alarm limits:

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2022