SCADAPack x70

Define the General Modbus Point Scanner Properties

These properties are included at the top of the Modbus tab on the configuration Form of a SCADAPack x70 Modbus Point Scanner:

In Service

Use to specify whether the Modbus Point Scanner is 'In Service' and included in the downloaded/exported configuration (see The 'In Service' Check Box and Items Taken Out of Service).

Modbus Server Device

Use to specify the Modbus Server Device with which the point scanner is associated.

Use the browse button to display a Reference browse window and then select the required entry from the window.


Disclaimer

Geo SCADA Expert 2022