SCADAPack x70

Display Modbus Point Scanners

Associated with: SCADAPack x70 Device Configuration items and SCADAPack x70 Modbus Server Devices

Security permission required to access this pick action: Read

Use the Display Modbus Point Scanners pick action to display a Queries List of SCADAPack x70 Modbus Point Scanners that are associated with the selected SCADAPack x70 Device Configuration item or SCADAPack x70 Modbus Server Device.

This pick action is not a method and therefore cannot be used with the automation interface.


Disclaimer

Geo SCADA Expert 2022