n <Object Name>
Associated with: SCADAPack x70 Object Browsers.
The n <Object Name> is a collection of status attributes numbered 1 to 'n'. These attributes list the entries in the selected Object Browser. The entries are those that are included in the configuration file that has been imported from RemoteConnect or the configuration that has been uploaded from the SCADAPack x70 device with which this Object Browser is associated.
Use these status attributes alongside the Number of Objects status attribute.
The following example shows the n <Object Name> status attributes of an Object Browser that includes information about 3 SCADAPack x70 object names. The names of the SCADAPack x70 objects are shown after the number that identifies the entry in the list that is stored in that Object Browser:
1 PIO_SP575_DI1
2 PIO_SP575_DI2
3 PIO_SP575_DI3
For information about Object Browsers, see Configure an Object Browser.