Debugging a Script
You can use Geo SCADA Expert’s Debug feature to check the validity of your script. This is a useful way of locating syntax errors and mistakes in your code that cause unexpected results.
The Debug feature is available for use with Mimic scripts and Alarm Banner scripts. To access it, you need to enable Debug Mode.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
The Debug feature is only available after you have installed the Microsoft Windows scd 10en.exe
feature. This feature is provided as a third-party application on your Geo SCADA Expert CD/DVD.