Define which Operational Features are Available to a User in ViewX and Virtual ViewX

The Operational settings on the ViewX tab allow you to restrict access to features in ViewX and Virtual ViewXonly. These settings have no effect on a user account when logging on via other types of client.

The properties described in this topic apply both to User Forms and User Pattern Forms. (User Patterns only apply to systems on which Geo SCADA Expert can create new User accounts automatically as part of an External Authentication process. For more information, see Create User Accounts from a User Pattern.)

The Operational settings on the ViewX tab allow you to define whether the user can execute methods on items in the database and view system alarms and events.

Use the Operational section of the ViewX tab to define which operational features are available when the user logs on from a ViewX or Virtual ViewX client. The section only lists operational features that you can set independently to those that apply when the user logs on via either a ViewX or Virtual ViewX client. For information about defining features that apply to both ViewX and Virtual ViewX, see Define the General Settings that Apply to ViewX and Virtual ViewX.

To define which operational features apply when the user logs on via a ViewX or Virtual ViewX client:

  1. Either:

  2. Select the ViewX tab.
  3. Define the Operational settings:

  4. Save the configuration.

Disclaimer

Geo SCADA Expert 2022