Web User Account

The Web user account is a built-in user account. It is used whenever a user accesses Geo SCADA Expert via a web interface such as Original WebX without logging on (see Original WebX Client). By default, the Web user has read-only permissions.

In some situations, the Web user may need specific permissions. For example, you may decide that web users need to be able to interact with alarms. To make this possible, you will need to configure the Web user account.

Virtual ViewX does not use this account and you must log on using a valid configured user account.

Further Information

Built-In User Accounts.

Configuring the Guest User Account.

Allocating Security Permissions.

User Account Created Automatically on the Virtual ViewX Server Machine.


Disclaimer

Geo SCADA Expert 2022