Alarm and Event Severities
In Geo SCADA Expert,
The default severities are Critical, High, Medium, and Low.
The default severity range meets the OPC
- 1000 is Critical.
- 667-999 is High.
- 334-666 is Medium.
- 1-333 is Low.
- 0 is used to indicate no severity and is an extension defined by Schneider Electric. It is not part of the OPC standard.
You can change the severity range to suit the requirements of your system, for example, you can add new severities so that the entire range is divided into more than 5 severity ranges.
The severities that you define are available for selection when configuring
We recommend that you add a separate Severity range, for example, if the points on your system are configured to raise an alarm whenever a change in a point's value results in the point reverting to its Normal state (see Return to Normal Alarm).
The Severity settings have to be identical on both servers in a hot-standby system and identical on the 3 servers in a triple-standby system.
Further Information
OPC Foundation Standards: See www.opcfoundation.org