Define the OPC HDA Server Limits

The Historic Configuration branch of the Geo SCADA Expert Server Configuration Tool contains a Historic Data section. This section includes the OPC HDA Server settings.

Each Geo SCADA Expert server has a built-in OPC HDA server. These settings enable you to define the OPC HDA Server limits for an item that is either a trace on a Historic Trend in ViewX, or has been created by a third-party OPC HDA client.

Use the section to set limits for the number of OPC HDA items that you can create. This can help to prevent denial of service due to OPC HDA clients creating an excessive number of items.

You configure the limits using the following settings:


Disclaimer

Geo SCADA Expert 2022