Remove a Historic Algorithm

You can use the Historic Algorithms section of the Geo SCADA Expert Server Configuration Tool to remove any unwanted custom algorithms.

To remove a historic algorithm:

  1. Access the Geo SCADA Expert Server Configuration Tool.
  2. Expand the Database Configuration branch on the tree-structure.
  3. Select Historic Algorithms.
  4. In the list, right-click on the historic algorithm that you want to alter.
    A context-sensitive menu is displayed.
  5. Select the Delete option.
  6. Close the Geo SCADA Expert Server Configuration Tool to apply the changes (or select another branch if further server configuration is required).

Now that you have modified the historic algorithm you can either proceed to configure other Historic settings (see Historic Configuration Settings) or you can continue with the server configuration.


Disclaimer

Geo SCADA Expert 2022