Specify the Duration to Retain Historic Data Online

The Keep online for field in the Geo SCADA Expert Server Configuration Tool's Historic settings allows you to specify the duration that Alarm Summary, Configuration Changes Auditing, Event Journal or Historic Data., is retained online. When this period of time expires, the historic data is deleted from the disk to allow space for the latest messages or data.

To configure the Keep online for duration:

  1. Access the Geo SCADA Expert Server Configuration Tool.
  2. Expand the Historic Configuration branch.
  3. Select the historical data type you require, Alarm Summary, Configuration Changes Auditing, Event Journal or Historic Data.
  4. Enter the amount of time (in weeks) for the historic data to be retained in the Keep online fornweeks field.

  5. When you have defined the Keep online for period:

Keep online for - Multi-server configuration

When you configure the server as part of a multi-server configuration the Keep online for period also defines the period that is synchronized between the servers, see Synchronization Process for Multi-Server Architectures.

When you configure the Keep online for period on a server as part of a multi-server configuration the Protect the Permanent Standby Servers when increasing online checkbox affects how space is allocated for historic data when you increase the value of the Keep online for period (see Protect the Permanent Standby Servers).

NOTICE

loss of data

When you extend the Keep online for period in a multi-server configuration you need to be aware of the effect of the Protect the Permanent Standby Servers when increasing online feature on the synchronization of data between Hot Standby Servers. If this is not carried out correctly you may lose online data.
Check the configuration of all your servers before they are restarted to avoid the loss of data.

The Index after setting can reduce the period that is synced between servers, see Manage the Size of the Primary Index. Data loss can still occur in certain scenarios for certain setting combination.

For more information about how this feature is affected by the other settings, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2022