OPC Status Information
The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. One of these groups is named OPC.
The OPC group provides status information about the OPC tags that are being used by clients connected to the server.
The OPC group contains the following sub-categories:
- .NET Tags—Reserved for use with future client applications.
- DA Groups—provides status information about the DA Groups to which a client subscribes.
- DA Items—provides status information about the OPC DA tags to which the OPC DA client(s) is subscribed.
- HDA Items—provides status information about the historic HDA tags to which the OPC DA client(s) is subscribed.
- XML-DA Items—provides status information about any XML-DA tags to which the OPC DA client(s) is subscribed.
- XML-DA Subscriptions—provides status information about XML-DA subscriptions. This information is often useful when determining whether Original WebX clients are being updated at a suitable rate.