About the Tutorial

The Geo SCADA Expert tutorial is designed to help first-time or inexperienced Geo SCADA Expert users get used to working in ViewX and Virtual ViewX (the two main Geo SCADA Expert user interfaces). Each section of the tutorial contains easy-to-follow instructions with explanations of the effects of your actions. As you work through the tutorial, you will learn about the common configuration procedures, displays, and methods used for accessing features.

Although each section includes instructions and helpful information, the tutorial is only designed to be a guide to Geo SCADA Expert and is not a substitute for the comprehensive online help documentation or a training course. Also, while the tutorial is aimed at first-time users, we recommend that users have a strong background in both programmable logic controllers (PLCs) and personal computers using Windows.

Throughout the tutorial, we have used the following conventions:

We recommend that you complete each of the tutorial sections in order, but if you wish to skip certain sections, you can do this. However, you may need to import files relating to the sections you have skipped. Instructions on how to import the files are included at the start of the sections.

Finally, if you are working on the tutorial and your system stops running, you will need to restart your server. This is because demo Geo SCADA Expert systems are set to stop running after 2 hours. For information on restarting the Geo SCADA Expert server, see Restarting your System.

If you are ready to start the tutorial, proceed to Using the ViewX Interface.


Disclaimer

Geo SCADA Expert 2022