Configuring TBox Historical Analog Points

Use the TBox Historical Analog Point Form to configure the properties that are specific to a TBox Historical Analog Point. For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.

You need to configure the parent TBox Analog Input Point or TBox Analog Output Point before you can save the Historical Analog Point. The Historical Analog Point is used to retrieve a Sampling Table associated with the parent point (see Sampling Tables).

Use the fields at the top of the tab to Configure Common Point Properties.

The following properties are specific to Historical Analog Points:

The other properties on this form are defined as for general Analog Points:


Disclaimer

Geo SCADA Expert 2022