Add a Web Page to your Favorites List

You can add web page links to your Favorites List. This allows you to access frequently used Internet or intranet sites from the ViewX Favorites List.

You might be asked to refrain from changing your Favorites while your Geo SCADA Expert system is in the process of being upgraded. For more information, see Upgrading Geo SCADA Expert.

To add a link to a website:

  1. Use one of the supported web browsers to open the website for which you want to add a link.
  2. Re-size the browser window and the ViewX window so that you can see the Favorites List in the ViewX window and the Address field of the browser window simultaneously.

  3. Select the icon next to the address on the browser window.
    Do not release the left-hand mouse button.

  4. Drag the icon onto the Favorites List in the ViewX window. (To add the icon to a folder in your Favorites List, drag the icon onto the relevant folder.)
  5. Release the left-hand mouse button.
    A link to the website is added to your Favorites List.


Disclaimer

Geo SCADA Expert 2022