Favorites Bar

The Favorites feature allows you to create and store links to those displays that you frequently use in your work. These links are stored in your Favorites List.

For example, by adding the Mimics, Lists, and Trends that you need to use on a frequent basis to your Favorites List (see Add a ViewX Display to your Favorites List), you can access those displays from the Favorites Barin ViewX, or the Links Bar in Virtual ViewX. You can also add web pages (see Add a Web Page to your Favorites List) and external documents (see Add an External File to your Favorites List) to your Favorites List.

Your Favorites List is associated with your user account. As such, if you log on to ViewX via a different computer, your Favorites are still in place. It also means that other users who log on to the same PC do not have access to your list of Favorite displays.


For information on how to display the Favorites Bar, see Display an Explorer Bar.

Further Information

Favorites


Disclaimer

Geo SCADA Expert 2022