Alarm Limits for WITS Analog Points

WITS analog points can have up to ten limits that you can configure to suit your requirements. The Device Profile defines how many limits a field device supports and also what types of limits are supported (see Display a WITS Device Profile).

Use the fields within the Alarm Limits section of the Analog Point tab to specify the properties for these alarm limits:

The upper part of the Alarm Limits section has a row of fields for each alarm limit. The number of rows you can use is defined by the Device Profile for your field device. The point Form shows the maximum number of available rows.

WITS specifies that the list of alarm limits is hierarchical, so the highest limit number has to have the highest limit value. For example, limit 5 has to have a higher limit value than limit 4, limit 4 has to have a higher limit value than limit 3 and so on. You also have to use the limits consecutively. For example, if your field device supports 3 limits, you use limits 1, 2 and 3.

The Normal state defines the usual operating range for the plant. This range will typically be between the lowest High value and the highest Low value.

Some types of analog point also have rows for the range limits Overrange, which is the maximum permitted value, and Underrange, which is the minimum permitted value.

Each limit is 1 incremental configuration record, and Overrange and Underrange share 1 incremental configuration record.

The following Alarm Limits properties are WITS specific:

The other Alarm Limits fields are common to many drivers (see Procedure for Configuring an Analog Point's Limits and see Define whether an Analog Point's Limits can be Tuned.

The availability of some of these settings, such as Hysteresis or Persistence, is dependent on your field device supporting that feature. For more details, see WITS Device Profiles.


Disclaimer

Geo SCADA Expert 2022