Procedure for Configuring an Analog Point’s Limits

Some analog points have different types of alarm limit to those mentioned in this guide. For example, the range supported by some analog points is Underrange to Overrange, rather than Zero Scale to Full Scale. The Procedure for Configuring an Analog Point’s Limits is typically similar, regardless of the type of limit. The driver guides explain any limits and configuration differences that are driver-specific.

To Configure the Limits for an Analog Point:

  1. Display the Form for the analog point that you want to configure.
  2. Select the Analog Point tab.
    (If you are configuring the limits for another point that uses analog-type processing, select the appropriately named <Point Type> tab. If you are configuring separate server-based limits, select the Master Station Alarm Limits tab.)
  3. Highlight the relevant Limit field. For example, if you are configuring the Full Scale, select the Limit field for the Full Scale row.

  4. Enter the required value. When you enter the value, you need to consider the requirements at the site. For example, if the analog point represents a thermometer, the point limits need to correspond to low/normal/high temperatures for the specific area of plant.

    With analog points on some drivers, you can optionally assign each limit to a Time Profile, to enable the limit’s value to change at different times of the day or week (see Specify any Alarm Limit Profiles). Whenever a limit is assigned a Time Profile, the Limit field within the Alarm Limits section of the Analog Point tab is ‘grayed out’. You still use the rest of the fields within the Alarm Limits section to specify other properties for the limit (such as the Severity, Description, or Color).

  5. Use the left-hand Severity combo box next to the Limit field to define what happens when the analog point’s value exceeds the limit (or for a limit below the Normal state, drops below the limit):

    • None—Geo SCADA Expert does not generate an alarm or event.
    • Alarm—Geo SCADA Expert generates an alarm. The alarm has the severity level that you select in step 6.
    • FleetingGeo SCADA Expert generates a fleeting alarm. The fleeting alarm has the severity level that you select in step 6. This option only is only available for the Normal state on points that support this feature.
      NOTICE

      UNEXPECTED BEHAVIOR OF APPLICATION

      Take care when configuring points to raise a fleeting alarm on transition back to the Normal state. Consider whether to configure such 'Return to Normal' alarms so that users are clearly able to distinguish between those alarms (which indicate a point's return to the normal operating state) and alarms that indicate an abnormal condition.
      Failure to follow these instructions can result in the unintended masking of the presence of other alarms.
    • Event—Geo SCADA Expert generates an event. The event has the severity level that you select in step 6.

      If you selected the Alarm, Fleeting or Event options, proceed to step 6.

      If you selected the None option, proceed to step 7.

  6. Use the right-hand Severity combo box next to the Limit field to define the level of importance associated with the event or alarm.

    A set of severity levels are provided for each Geo SCADA Expert system (see Defining Severities in the Geo SCADA Expert Guide to Core Configuration). Choose the appropriate severity level from the list available on your system.

    If any of the analog points on your system have Multiple Point State Alarms configured, an additional Alarm column is displayed to the left of the Description combo box. For information on specifying multiple Alarm Conditions, see Multiple Point State Alarms.

  7. Use the Description combo box to enter or select a suitable description of the limit.

    You can either highlight the existing description and replace it with a new one, or you can choose one of the available d escriptions from the combo box list. There are default descriptions for each limit, but these can be replaced by user-defined descriptions that are more specific to the points on your system (see Define Descriptions for Numeric Point States in the Geo SCADA Expert Guide to Server Administration).

    Usually, the Description describes the state of the plant or conditions at the site. For example, with an analog point that represents a sensor at a reservoir, the description for a High-High limit might be ‘Flooding’. The description provides extra information to operators so that they have a better understanding of what the High-High limit represents.

    If the Dictionary feature is used on your system, you can prefix the string in Description field, in order for that string to be replaced with another term, when displayed in a List or on a Mimic, in ViewX. For more information, see Introduction to the Geo SCADA Expert Translation Dictionary in the Geo SCADA Expert Guide to the Translation Dictionary.

    By default, point states are shown in black text on displays such as Lists, unless:

    • The point is in an alarm state (in which case the text is displayed in the corresponding severity color)
    • Another status, such as an Override, takes precedence over a non-alarm state (in which case the text is displayed in the color that indicates that status).

      You can change the color that your system uses for the ‘Normal’ state (black by default), using the Color Palette (see Use the Color Palette to Define a Custom System Color in the Geo SCADA Expert Guide to Core Configuration).

      If you want to associate a state with a custom color when neither of the above situations is in effect, proceed to step 8.

      If you want the state to use the default color to indicate a ‘Normal’ state (black by default), proceed to step 10.

  8. You can only associate a limit with a custom color if you have pre-configured custom colors available (see Defining a Custom State Color in the Geo SCADA Expert Guide to Core Configuration). To use the Color field to associate the limit with a custom color:
    1. Select the browse button next to the Color field for the limit you are configuring.
      A Reference browse window is displayed.

    2. Use the Reference browse window to locate the required custom color.
    3. Select the custom color.
    4. Select the OK button.
      The Reference browse window is closed and the name of the selected color is shown in the Color field. When the point enters this state, its value will be shown in the custom color.
  9. Repeat steps 3-8 inclusive for each limit.
  10. Save the configuration.

If the Area of Interest feature is enabled on your system, also ensure that you Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events.


Disclaimer

Geo SCADA Expert 2022