Alarm Limits for WITS Integrator Points

You need to set the alarm limits for each WITS Integrator Point so that when the value of the point rises above the normal range of values, Geo SCADA Expert raises a suitable alarm or logs an event.

WITS Integrator points can have up to ten alarm limits that you can configure to suit your requirements. The Device Profile defines how many alarm limits a field device supports (see Display a WITS Device Profile).

Use the fields within the Alarm Limits section of the Integrator tab to specify the properties for these alarm limits.

The WITS Integrator Point has a base type of Analog Input. Therefore, many of theAlarm Limits fields for the point are the same as those for other WITS analog points (see Alarm Limits for WITS Analog Points).


Disclaimer

Geo SCADA Expert 2022