End Point for WITS Network Connections

If your WITS Field Device communicates with Geo SCADA Expert via a network connection, the connection has to be initiated by either Geo SCADA Expert or the Field Device. Depending on your requirements, you can configure your WITS Field Device so that:

Some Field Devices may not support all of the connection types listed above. For information on the connection types supported by your Field Device, please refer to its Device Profile (see Display a WITS Device Profile)

To define whether a connection can be initiated by Geo SCADA Expert, your Field Device, or both, you need to use the End Point settings. These are located on the Network tab of the WITS Outstation Form.

End Point Settings on WITS Outstation Form (Network tab)

The End Point types that are available are defined by the Device Profile for your Field Device (see Display a WITS Device Profile). They also vary, depending on the Device Port (see Device Ports for WITS Field Devices).

The End Point setting at the top of the Network tab is for defining the outbound connection (from Geo SCADA Expert to the Field Device). If a Dual Network is used, there are outbound connection End Point settings for each network.

You can set the outbound connection End Point(s) to:

The End Point settings in the Inbound Connection section of the Network tab relate to the inbound network connections (Field Device to Geo SCADA Expert). You can set the End Point(s) to:

 

If a Field Device:

You need to configure both outbound network connections to have an End Point type of Listening. In this scenario, there are no incoming connection settings required.

Listen Only with Network Redundancy

If a Field Device supports 'listening' and initiating via separate connections (does not support End Point: Dual), you need to configure:

WITS Field Device Listen on one Network Connection, Initiate another

If a Field Device supports 'listening' and initiating via the same connection, you need to configure the inbound and outbound connections to have Dual End Points.

Dual End Points Inbound and Outbound Network Connections

Further Information

Configure a WITS Field Device to Initiate Only

Configure a WITS Field Device to Listen Only

Configure a WITS Field Device to Listen and Initiate via the Same Connection

Configure a WITS Field Device to Listen and Initiate via Separate Connections.


Disclaimer

Geo SCADA Expert 2022