Export Configuration

Associated with: WITS Outstations.

Security permission required to access this pick action: Configure.

Geo SCADA Expert stores the bulk configuration file for your WITS Field Device, and can also create an incremental configuration file that contains the configuration settings you make in Geo SCADA Expert. To use these files externally, for example, in a vendor-supplied configuration tool, you need to export them from Geo SCADA Expert. To do this, you need to use the Export Configuration action for a WITS Outstation.

When exporting a bulk configuration file, it is good practice to include the version in the file name. (If you do not include the version, it may lead to confusion if the file is imported at a later date). If you are not aware of the version for the bulk configuration file currently stored in Geo SCADA Expert, access the View Status dialog box for the WITS Outstation item (look for Bulk Configuration Version).

When you select Export Configuration for a WITS Outstation, an Export Configuration window is displayed.

WITS Outstation - Export Configuration

It prompts you to select an Incremental Configuration File and a Bulk Configuration File:

You can use the browse buttons for both fields to define the location to which the configuration files will be exported.

When you select the OK button, Geo SCADA Expert saves the configuration files in the locations you specified. They can now be used in external applications.


Disclaimer

Geo SCADA Expert 2022