Bulk Configuration File - Content and Syntax

WITS Field Devices take their configuration from a bulk configuration file, which can be:

When saving a bulk configuration file in a Configuration Application, or exporting a bulk configuration file from Geo SCADA Expert, you need to use the correct filename syntax.

The WITS-DNP3 standard defines the bulk filename syntax as:

<name>_<version>.<extension>

Where:

For example:

BVPump1_20080107.bcf

MPReservoir_V32.dat

Further Information

Bulk Configuration and Incremental Configuration Files - Generation and Transfer

Incremental Configuration File - Content and Syntax

WITS Configuration Strategies


Disclaimer

Geo SCADA Expert 2022