Import Configuration
            Associated with: WITS Outstations.
Security permission required to access this pick action: Configure.
INCORRECT CONFIGURATION
You can use the Import Configuration pick action to import a WITS Field Device's configuration into Geo SCADA Expert. Typically, you will need to use the Import Configuration pick action as part of your chosen configuration strategy (see WITS Configuration Strategies)
If you are going to import the configuration, and the Outstation or any of its points or profiles are in a Group Instance, you need to be aware of:
- Property Overrides
                    
If the necessary Property Overrides are not defined, Geo SCADA Expert will be unable to write the changes to the database and the import process will be unsuccessful. For more details, see Property Overrides.
 - The Point Conversion Process
                    
As part of the import process, Geo SCADA Expert may need to change the type of existing points in the Geo SCADA Expert database. For example, it may convert an Analog Input into a Minimum point so that it matches the configuration being imported. This conversion cannot take place if the point is in a Group Instance, as its type is determined by the matching point in the Group Template. For more details, see Importing/Uploading Configuration - Point Conversion.
 
If an import fails as a result of missing Property Overrides or point conversions being required, Geo SCADA Expert lists the configuration errors in a configuration report (see Configuration Reports for WITS Field Devices). There are no changes made to the Geo SCADA Expert database.
When you select the Import Configuration action, the Import Configuration window is displayed. It contains the relevant combination of these fields:
                
            
The window contains the following fields:
- 
                    
Mode—Use to specify whether the imported configuration will overwrite any existing configuration changes (for the WITS Outstation and its points and profiles in the Geo SCADA Expert database).
Choose Merge if you want Geo SCADA Expert to preserve any changes you have already made to the configuration (in Geo SCADA Expert). When Geo SCADA Expert merges the new configuration (being imported) with the current configuration (in the database), it only updates those incremental configuration records that have not already been modified. If any part of a record has already been changed in Geo SCADA Expert, the entire new record will be discarded and the existing changes preserved. For details on the incremental configuration records, see Incremental Configuration File - Content and Syntax.
For example, let's say you import the initial configuration for a Field Device into Geo SCADA Expert and then change an alarm limit for an analog point (in the Geo SCADA Expert database). When you initiate the next import configuration, selecting Merge will mean that Geo SCADA Expert will detect that the alarm limit has been modified. It will import every incremental configuration record except the record for the alarm limit that was changed.
Choose Replace if you want the imported configuration to overwrite the entire configuration that is already in place for the Outstation, its points and its profiles.
Choose WITS Files Only if you only want to import bulk configuration and incremental configuration files into the Geo SCADA Expert database. When you select this option and import the configuration, Geo SCADA Expert does not create any new points or overwrite the existing configuration of the points or profiles. When you use this mode to import configuration, any existing points or profiles in the database that don't exist in the imported configuration will become invalid (this is by design, to help prevent them from being downloaded in future).
When the Mode is set to Merge or Replace, if the import includes configuration that does not exist in Geo SCADA Expert, Geo SCADA Expert creates the appropriate items and configuration automatically. If the configuration already exists in the Geo SCADA Expert database, Geo SCADA Expert just updates the configuration settings to match those of the import.
 - Incremental Configuration File—Choose the incremental configuration file to import. This is the incremental configuration file that matches the bulk configuration file and is created by using a Configuration Application.
 - 
                    
Bulk Configuration File—Choose the bulk configuration file to import. This file is created by using a Configuration Application and its filename has to have the correct syntax for the import to succeed (see Bulk Configuration File - Content and Syntax).
If your Field Device does not support configuration download, the Bulk Configuration File field is not shown.
 
When you select the OK button, Geo SCADA Expert begins the import process. If the Mode is set to Merge or Replace, it updates/replaces the existing configuration for the Field Device's Outstation, Points and Profiles using some or all of the configuration from the imported incremental configuration file. If the Mode is set to WITS Files Only, it does not create any new points or profiles, or overwrite the existing configuration. However, any points or profiles that exist in the Geo SCADA Expert database but not in the imported configuration will become invalid.
If the import process is unsuccessful, no changes are made to the configuration and an error report is generated. The report indicates the reasons for the import failure (see Configuration Reports for WITS Field Devices).