Rules for Using Time Profiles for Limit Profiles with WITS Database Points

If you want to configure variable limits for a WITS analog point or counter point, you will need to use one or more Time Profiles. While Time Profiles can be used by several Geo SCADA Expert drivers, there are certain rules that you need to follow when using them with WITS. The rules differ, depending on the type of WITS database point.

 

For analog points (and integrator points and rate-of-change points):

 

For counter points:

 

For state counter and state runtime points:


Disclaimer

Geo SCADA Expert 2022