Configure the Background Color and Drawing Mode

You can change an X-Y-Z Plot's background color and the mode in which data is shown on the plot. You do this using fields in the X-Y-Z Plot Properties window (see Change the Appearance of an X-Y-Z Plot).

Use the Miscellaneous section of the window to specify these properties:

Examples:

An X-Y-Z Plot showing data in 'Connect by Point' mode:

The same data shown in 'Connect by Timestamp' mode:

The same data shown in 'Connect by Point and Timestamp' mode:


Disclaimer

Geo SCADA Expert 2022