Configure the Line and Marker Properties when in 'Connect by Point' Mode

The means by which you specify the properties that are associated with a trace's line and markers varies, depending on the X-Y-Z Plot's 'Drawing Mode' (see Configure the Background Color and Drawing Mode). When the 'Drawing Mode' is set to 'Connect by Point', you configure the properties using fields in the Trace Properties window. For information on displaying the Trace Properties window, see Configure a Trace.

(When a Drawing Mode other than 'Connect by Point' is selected, the fields shown below are 'grayed out' and unavailable for use in the Trace Properties window.)

Use the Line section of the window to specify these properties:

Use the Markers section of the window to specify these properties:

To view an example of an X-Y-Z Plot showing data in 'Connect by Point' mode: see Configure the Background Color and Drawing Mode.


Disclaimer

Geo SCADA Expert 2022