Show or Hide the Whole Trace Entry

NOTICE

UNEXPECTED BEHAVIOR OF APPLICATION

You can hide a trace's content in Run or Design mode. If you are working in Design mode, ensure that the required trace content remains on show when saving the plot's configuration. Content that is hidden when the configuration is saved will continue to remain hidden from view by default.
Failure to follow these instructions can result in data being omitted from display unintentionally

You can show of hide the content that is associated with a trace—this includes the trace's label, markers, slice fill color, and (if applicable) the trace line. (A line is only drawn between trace values when an X-Y-Z Plot's Drawing Mode is set to 'Connect by Point' or 'Connect by Point and Timestamp' (see Configure the Background Color and Drawing Mode).)

To hide the content that is associated with a trace:

  1. Right-click on the tick (short line) that indicates the trace's position on the x-axis.
    A context-sensitive menu is displayed
  2. Select the Show option.
    A further context-sensitive menu is displayed.
  3. Select the None option.
    The content that is associated with the trace is omitted from the X-Y-Z Plot. The x-axis retains the tick that indicates the hidden trace's position. If the X-Y-Z Plot uses one of the 'Connect by Timestamp' Drawing Modes, the lines that link the surrounding data values are redrawn to omit reference to the hidden set of data.

To show the content that is associated with a currently hidden trace:

  1. Right-click on the tick (short line) that indicates the hidden trace's position on the x-axis.
    A context-sensitive menu is displayed
  2. Select the Show option.
    A further context-sensitive menu is displayed.
  3. Select the All option.
    The content that is associated with the selected trace entry is shown on the X-Y-Z Plot. This includes the trace's label, markers, slice fill color, and (if applicable) the trace line. If the X-Y-Z Plot uses one of the 'Connect by Timestamp' Drawing Modes, the lines that link the surrounding data values are redrawn to take into account the redisplayed set of data.

As an alternative to selecting the 'All' option, you can opt to redisplay just a subset of the trace's content, such as just the markers or trace label (see Show or Hide the Content that is Associated with an Individual Trace). Again, if applicable, Geo SCADA Expert will redraw the lines that link the surrounding data values to take into account the redisplayed subset of data. This applies if you do opt to redisplay a previously hidden trace line, set of markers, or slice fill color and the X-Y-Z Plot uses one of the 'Connect by Timestamp' Drawing Modes.

Example:

An X-Y-Z Plot showing four sets of data:

The same X-Y-Z Plot after the set of data associated with 'Sensor 3' has been hidden using the 'None' option. Geo SCADA Expert has redrawn the lines that link the surrounding data values so that the lines omit reference to the hidden set of data. (The tick (short line) that indicates the hidden trace's position remains visible on the x-axis, so that the hidden set of data can be redisplayed when required.)

If you are working with an X-Y-Z Plot in Design mode, consider whether you want to permanently Remove a Trace that is no longer required.


Disclaimer

Geo SCADA Expert 2022