Configure a VT Service Port Slave

A VT Service Port Slave allows a DNP3 Virtual Terminal to transfer data transparently between a port on the ClearSCADA server DNP3 master, via a DNP3 Slave outstation item configured in the ClearSCADA database.

Where more than one port is used on a Slave outstation, you need to configure one VT Service Port Slave for each port.

Configure the service port settings using the VT Service Port Slave Form. The Form has several tabs.

Use the Connection tab to define the connection-specific settings for the port. The port uses serial communications (see Configure a Channel’s Serial Connection Properties in the ClearSCADA Guide to Advanced Drivers).

Use the Slave VT Port tab to:

The properties on the other tabs are common to many database items. For information on these properties, see Tabs that are Common to Many Configuration Forms in the ClearSCADA Guide to Advanced Drivers.


Disclaimer

ClearSCADA 2017 R2