Configure the Profiler and ISaGRAF Time Zone Properties

Use the Time Zone field towards the bottom of the SCADAPack tab to specify the time zone that is used for the SCADAPack E outstation’s Profiler and ISaGRAF functions. This time zone is independent of the time zone used for the SCADAPack E outstation’s internal clock.

The outstation’s internal real-time clock is set to Coordinated Universal Time (UTC) by the NTP service (see Enable TCP/IP Services), or to UTC or Local Time (whichever is required) by ClearSCADA issuing DNP3 Write Time requests. Most outstation functions, including DNP3 event time stamps, use the time zone that is assigned to the outstation’s clock. For these functions, this Time Zone field has no effect. Only a few specific ISaGRAF function blocks and the SCADAPack E outstation’s Profiler task use a time zone that is independent to that of the outstation’s clock (that is, the time zone specified using this Time Zone field). For further information, see the SCADAPack E Operation Reference Manual.

 

Further Information

Specify the Profile Type.

Time Zone property: see Time Zone Support in ClearSCADA in the ClearSCADA Guide to Core Configuration.


Disclaimer

ClearSCADA 2017 R2