Enable TCP/IP Services

By default, only DNP3 communications over UDP and TCP are enabled on a SCADAPack E outstation. A number of other TCP/IP services are available on the outstation.

Use the Enabled TCP/IP Services fields on the SCADAPack TCP/IP tab to specify those IP services that are required on the SCADAPack E outstation.

For each service that is required, select the relevant check box so that it displays a check mark. Ensure that a check box is clear for any services that are not required. The services that you can choose from are:

For more information on any of these IP services, see the documentation supplied with the SCADAPack E outstation.


Disclaimer

ClearSCADA 2017 R2