Display the Table

To display a BOOTP, IP Route, or DNP Route Table in Design mode, so that you can alter its configuration:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Either:
    • Double-click on the table in the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature enabled.

    Or:

    1. Right-click on the BOOTP, IP Route, or DNP Route Table in the Database Bar.
      A context-sensitive menu is displayed.
    2. Select the Edit <Table type> option, for example for a DNP Route Table select Edit SCADAPack DNP Route Table.

      The table is displayed as a series of rows and columns, as shown below.

While a table is displayed in Design mode, you can:

Further Information

Route DNP3 Frames Using a DNP Route Table.

Use an IP Route Table to Route TCP/IP Packets to Another TCP/IP Host.

Types of IP Route.


Disclaimer

ClearSCADA 2017 R2