Security Description

Associated with: DNP3 SCADAPack Security Configuration items.

This status attribute indicates the description that was entered for the security configuration file when it was imported into the ClearSCADA database (see Import Security Configuration).

Use this status attribute in conjunction with the Security File attribute to ascertain information about the security configuration file with which this particular DNP3 SCADAPack Security Configuration item is associated.


Disclaimer

ClearSCADA 2017 R2