Security File
Associated with: DNP3 SCADAPack Security Configuration items.
This status attribute indicates the name of the security configuration file that was last imported into ClearSCADA using this particular DNP3 SCADAPack Security Configuration item (see Import Security Configuration). The date and time that the file was last modified is also shown. (To ascertain the date and time that the file was imported into ClearSCADA, see the Events List.)
Use this status attribute in conjunction with the Security Description attribute to ascertain information about the security configuration file with which this particular DNP3 SCADAPack Security Configuration item is associated.
Example:
"system.rtk" Modified at May/06/2010 14:27:00.000