Configure the Forecast Properties
To configure the Forecast properties, you need to display the Forecast Form (see Display a Form).
The Forecast Form has these tabs:
- Identification—Use to configure the Identification properties (see Defining Identification Details).
-
Location—Use to specify the item's geographical coordinates. (You need only configure the properties on this tab if your system uses ClearSCADA's Geographical Location features.)
- User Methods—Use to define any custom pick actions (‘methods’) for the Forecast (see Using the User Methods Tab to Define Custom Actions).
- Alarm—Use to define optional features associated with any Forecast alarms (see Defining an Item or Group’s Alarm Properties).
- Redirection—Use to define any alarm redirections for the Forecast (see Configure Alarm Redirections for an Item or Group in the ClearSCADA Guide to Alarm Redirection).
- Forecast—Use to configure the Forecast-specific properties. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
If the Area of Interest feature is enabled on your system, an additional Area of Interest field is displayed toward the top of the Forecast tab. Use the field to specify the area with which any Forecast alarms or events are to be associated (see Assign a Different Area of Interest to an Item’s Alarms and Events).
For further information on the Area of Interest feature, see Restrict Alarm and Event Access to Specific Areas of Interest.