Configure an Output Point or Pulse Action’s Interlock Properties

For each DNP3 SCADAPack Output point that ClearSCADA is to control exclusively, or for which point control alters between ClearSCADA and ISaGRAF, ensure that the point’s Control aggregate is enabled (see Specify Whether an Output Point is Controlled by ClearSCADA in the ClearSCADA Guide to the DNP3 Driver).
For each DNP3 SCADAPack Output point that is controlled exclusively by another application, rather than ClearSCADA, you need to disable that point’s Control aggregate. For such points, fields on the Control tab are unavailable for use and you can ignore the rest of this section.

In addition to the properties that are common to DNP3 Output points (see Configure the DNP3-Specific Control Properties on DNP3 Output Points in the ClearSCADA Guide to the DNP3 Driver), DNP3 SCADAPack Output points have the properties that are described below. The properties below also apply to DNP3 SCADAPack Pulse Actions.


Disclaimer

ClearSCADA 2017 R3