Restart Level

When a file is added to the ClearSCADA database, ready for downloading to a SCADAPack E outstation, the action that ClearSCADA is to perform following the downloading of that file is specified in the Re-Start Level column of the Configuration Setup Window.

The following Restart Levels are available:

For restart levels not listed above, see Determine the Restart Level of a Configuration Download.


Disclaimer

ClearSCADA 2017 R3