Download Parameters

Associated with: Sofrel S500 Series Outstations.

Security permission required to access this pick action: Configure.

The Download Parameters action is available for Sofrel S500 series outstations using the LACBUS-RTU protocol. These outstations are pre-configured before being connected and setup within ClearSCADA. You can use ClearSCADA to modify parameters within the outstation configuration and this action allows you to download the parameter changes to the outstation.

If the Call Recipients feature is disabled in ClearSCADA then this pick action is not available.

When you select the Download Parameters action the Download Parameters dialog box is displayed.

Use the Download combo box to select one of the following options:

Select OK to initiate the download.

Call Recipients are currently the only parameters that are supported by ClearSCADA.


Disclaimer

ClearSCADA 2017 R3